Technical FAQs

Ask a Question

What handle is used with the 9422RX1?

Use the 9422A1 for NEMA 1, 3R, 4, and 12 sheet steel enclosures. Use the 9422A2 for types 4, and 4X stainless steel.


CTA-ID : 2019523
Was this helpful?
What can we do to improve the information ?