Technical FAQs

Ask a Question

Are alternate lugs available for a D223NRB safety switch to accommodate (2) conductors per phase?

ISSUE:
Alternate Lugs

PRODUCT LINE:
General Duty Safety Switches

ENVIRONMENT:
Alternate Lugs

CAUSE:
Change in Wire Size

RESOLUTION:
No, this switch is UL listed with the standard lugs supplied, which accommodate (1) #12-1 AL or (1) #14-1 CU AWG conductors per phase. Alternate lugs have not been tested nor listed for use on the switch.



CTA-ID : 2019233
Was this helpful?
What can we do to improve the information ?