Technical FAQs

Ask a Question

What does the S276 suffix at the end of an ATV58 part number indicate?

This drive was only available in Europe and was not available in the United States. The S276 indicated that the drive had some programming functionality that was not available on the standard ATV58 without this S276 suffix. This programming functionality has been incorporated on all ATV58 drives since 3rd quarter 2000. Therefore the S276 suffix is no longer needed when ordering an ATV58 drive.




CTA-ID : 2020180
Was this helpful?
What can we do to improve the information ?