Technical FAQs

Ask a Question

Will the QO403L60NS/F/RB load centers accept a QO, 3 pole breaker with an electrical accessory, like a shunt trip?

Issue:
Product design features

Product line:
QO three phase load centers

Environment:
Branch breakers with accessories

Cause:
Application

Resolution:
Yes, using a QO360 or less


CTA-ID : 2019770
Was this helpful?
What can we do to improve the information ?