Technical FAQs

Ask a Question

What lug can I use on the FAL34100?

Issue:  
What is the part number for a standard lug kit for a FAL breaker?

Product line:  
Molded case circuit breakers

Environment:  
FA, FAL, FH, FHL Legacy molded case breakers

Resolution:  
The standard lug is AL100FA. Optional copper, compression, and Power Distribution (PDC) lugs are also available.
Was this helpful?
What can we do to improve the information ?