Technical FAQs

Ask a Question

What are the Nema and IEC ratings of the XUL photo type sensors?

Nema 1,3,4,6,6P,12, and 13.
IEC IP67


CTA-ID : 2019513
Was this helpful?
What can we do to improve the information ?