Technical FAQs

Ask a Question

Customer has a 150HP motor at 480V and they want the correct size circuit breaker.

Per motor selection table in the Digest, they can use a 250A LA if the motor is ordinary service. See digest for heavy service or high efficiency.


CTA-ID : 2020120
Was this helpful?
What can we do to improve the information ?