Technical FAQs

Ask a Question

What is the maximum current rating of a QO circuit breaker that can be installed into a QO2100BNF?<br />

The maximum QO breaker size is a 2pole,100amp.


CTA-ID : 2019754
Was this helpful?
What can we do to improve the information ?