Technical FAQs

Ask a Question

Can a 225A NQOD standard main breaker panel be field converted to a non-linear panel with thru-feed lugs by ordering a non-linear, main lug, thru-feed interior and moving the main breaker kit to the new panel?

No, the panel cannot be converted. Issues with this are: the non-linear main breaker deadfront is different than a standard main breaker deadfront and the main breaker would have to K frame type.

CTA-ID : 2019751
Was this helpful?
What can we do to improve the information ?