Technical FAQs

Ask a Question

What are the repair parts for the HU361DSWC, series F7 (may be shown as F07)?

The repair parts for the HU361DSWC, series F7 (F07) are as follows. No other parts are available.

-Line Base Assembly - 4056609150 (requires one. Arc Suppressor not included)
-Line and Load Base Mounting Screws - 4020515101 (3 required)
-Arc Suppressor Assembly - 4056635550 (requires one)
-Arc Suppressor Mounting Screw - 4020514501 (requires one)
-Lug Assembly - 4025101652 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056646950 (NOTE: Handle Coupling, Cover Interlock Defeat Coupling, and Lockplate Gaskets may also need replacing)
-Handle Coupling - 4053922550
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056779850 (also recommend replacing Lockplate Gaskets)
-Lockplate - 4056681201 (also recommend replacing Lockplate Gaskets)
-Lockplate Gasket - 4050322802 (2 required)
-Lockplate Mounting Screw 2194918121 (2 required)
-Rod/Linkage Assembly - 4056787050
-Receptacle - 25410-000-45
-Receptacle Mounting Screws - 45102-801-01
-Ground Lug - 4025101652 (3 total required)
-Ground Lug Mounting Screw - 4020513503 (2 total required)


CTA-ID : 2019489
Was this helpful?
What can we do to improve the information ?