Technical FAQs

Ask a Question

What are the repair parts for the H363DSWC, series F7 (may be shown as F07)?

The repair parts for the H363DSWC, series F7 (F07) are as follows. No other parts are available.

-Line Base Assembly - 4056775150 (requires one. Arc Suppressor not included)
-Load Base Assembly - 4056602850 (requires one)
-Line and Load Base Mounting Screws - 4020515101 (3 for line, 2 for load)
-Arc Suppressor Assembly - 4056635550 (requires one)
-Arc Suppressor Mounting Screw - 4020514501 (requires one)
-Lug Assembly - 4025101852 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056646950 (NOTE: Handle Coupling, Cover Interlock Defeat Coupling, and Lockplate Gaskets may also need replacing)
-Handle Coupling - 4053922550
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056779850 (also recommend replacing Lockplate Gaskets)
-Lockplate - 4056681201 (also recommend replacing Lockplate Gaskets)
-Lockplate Gasket - 4050322802 (2 required)
-Lockplate Mounting Screw - 2194918121 (2 required)
-Rod/Linkage Assembly - 4056787150
-Receptacle - 25410-000-47
-Receptacle Mounting Screws - 45102-801-01
-Ground Lug - 4025114801 (3 total required)
-Ground Lug Mounting Screw - 4020514801 (longer screw) and 4020513503 (shorter screw) - 1 each
-Fuse Pullers - FPK0610 (1 required)



CTA-ID : 2019487
Was this helpful?
What can we do to improve the information ?