Technical FAQs

Ask a Question

What neutral assembly is used on a single row HCP-SU I-Line interior when main lugs are provided or a main breaker without ground fault?

The neutral assembly would be an HCPSU8SN.


CTA-ID : 2020103
Was this helpful?
What can we do to improve the information ?