Technical FAQs

Ask a Question

What are the lug wire sizes on the QOM2-MM and QOM2-MVH tenant breakers use in the MP Meter-Pak product line?

The lugs will accept wire sizes #4awg through 300kcmil AL/CU.


CTA-ID : 2019744
Was this helpful?
What can we do to improve the information ?