Technical FAQs

Ask a Question

What are the repair parts for the H362DSWC, series F7 (may be shown as F07)?

Issue:
Current Design repair parts

Product Line:
Heavy Duty Safety Switches

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The repair parts for the H362DSWC, series F7 (F07) are as follows. No other parts are available.

-Line Base Assembly - 4056603850 (requires one. Arc Suppressor not included)
-Load Base Assembly - 4056604050 (requires one)
-Line and Load Base Mounting Screws - 4020515101 (3 for line, 2 for load)
-Arc Suppressor Assembly - 4056635550 (requires one)
-Arc Suppressor Mounting Screw - 4020514501 (requires one)
-Lug Assembly - 4025101652 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056646950 (NOTE: Handle Coupling, Cover Interlock Defeat Coupling, and Lockplate Gaskets may also need replacing)
-Handle Coupling - 4053922550
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056779850 (also recommend replacing Lockplate Gaskets)
-Lockplate - 4056681201 (also recommend replacing Lockplate Gaskets)
-Lockplate Gasket - 4050322802 (2 required)
-Lockplate Mounting Screw 2194918121 (2 required)
-Rod/Linkage Assembly - 4056787050
-Receptacle - 25410-000-46
-Receptacle Mounting Screws - 45102-801-01
-Ground Lug - 4025101652 (3 total required)
-Ground Lug Mounting Screw - 4020513503 (2 total required)
-Fuse Pullers - FPK0610 (1 required)


CTA-ID : 2019485
Was this helpful?
What can we do to improve the information ?