Technical FAQs

Ask a Question

If an LAL breaker is tripped when using an LAMO1 motor operator, can you reset the breaker using the motor operator?

Yes. Turning the breaker off and then on again with the motor operator resets the breaker.


CTA-ID : 2020097
Was this helpful?
What can we do to improve the information ?