Technical FAQs

Ask a Question

What are the repair parts for a QMJ365, Series E2 (E02)?

Issue:
Current design repair parts

Product line;
Heavy Duty Safety Switches

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable:

Arc Suppressor Assembly (3 per switch) - 40520-289-50
Load Base Assembly (3 per switch, does not include lugs) - 40521-089-50
Handle Knob Kit - 40283-436-50
Lug Assembly (per lug) - 40251-136-50
Lug Mounting nut (per lug) - 23427-024-00
Load Base Mounting Screw (3 required per load base) - 40205-065-01


CTA-ID : 2020094
Was this helpful?
What can we do to improve the information ?