Technical FAQs

Ask a Question

What is the torque for the 4/0 to 350 MCM lug on the NJNL36250 breaker?

It is 31 Nm or 275 lb.-in.


CTA-ID : 2020089
Was this helpful?
What can we do to improve the information ?