Technical FAQs

Ask a Question

What is the main wire size for a PAK10CTG?

This main terminals on this device will accept (1) #14 - 6 AWG CU or (1) #12 - 6 AWG AL. A second set of loop feed terminals, with the same wire range as the main terminals, is provided for loop feeding the conductors.

CTA-ID : 2019726
Was this helpful?
What can we do to improve the information ?