Technical FAQs

Ask a Question

What is the Main wire size for a PAK75CTG?

The main terminals on this device will accept (1) #14 - #1 AWG CU or (1) #12 - #1 AWG AL. This device does not have loop feed terminals available.



CTA-ID : 2019724
Was this helpful?
What can we do to improve the information ?