Technical FAQs

Ask a Question

What are the amperage choices for a QOM1 type breaker.

50A, 60A, 70A, 80A, 90A, 100A, 110A, 125A.


CTA-ID : 2019719
Was this helpful?
What can we do to improve the information ?