Technical FAQs

Ask a Question

What is a acceptable megger reading for safety switches.

UL standards do not specify an acceptable megger reading. UL standards require a dielectric voltage withstand test be conducted at twice rated voltage plus 1000V for one minute ( phase to phase and phase to ground).
A reading of less than 1 meg ohm should be investigated as a possible `` unsafe condition``.


CTA-ID : 2020075
Was this helpful?
What can we do to improve the information ?