Technical FAQs

Ask a Question

Can the cover of a MA1000F, Series E01, E02 or E03 flush mount circuit breaker enclosure be changed to adapt the enclosure to a surface mount application?

The cover from a MA1000S will physically fit onto the MA1000F enclosure. A replacement cover ordered as a repair part would not include any labeling nor wiring diagram. Since the UL manifest is located on the wiring diagram, this change is not recommended.

CTA-ID : 2019693
Was this helpful?
What can we do to improve the information ?