Technical FAQs

Ask a Question

Do we have an rotary handles for the Powerpact P frame breaker?

P-frame and NS630b?NS1600 circuit breakers are available with factory-installed rotary handles. The
handles are available in standard black directly-mounted, door-mounted or telescopic door-mounted
versions. The rotary handles are available with two early-break or two early-make contacts.

CTA-ID : 2019446
Was this helpful?
What can we do to improve the information ?