Technical FAQs

Ask a Question

Is the HPAFK handle lockoff UL approved?

Since there are no specific standards for these, they are UL acknowledged and do not impair the UL listing of the circuit breaker.


CTA-ID : 2020061
Was this helpful?
What can we do to improve the information ?