Technical FAQs

Ask a Question

What are the repair parts for the HU362AWA, series F7 (may be shown as F07)?

The repair parts for the HU362AWA, series F7 (F07) are as follows. No other parts are available.
-Line Base Assembly - 4056609150 (requires one. Arc Suppressor not included)
-Line Base Mounting Screws - 4020515101 (3 total required)
-Arc Suppressor Assembly - 4056635550 (requires one)
-Arc Suppressor Mounting Screw - 4020514501 (requires one)
-Lug Assembly - 4025101652 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056787350 (NOTE: also recommend replacing Switch Mechanism Gasket and Handle Gasket)
-Switch Mechanism Gasket - 4056786001
-Mechanism Washer - 2360200008
-Handle Assembly - 4056663550 (also recommend replacing Handle Gasket)
-Handle Gasket - 4056603101
-Lockplate - 4056672101
-Lockplate Mounting Screw - 2299940562 (2 required)
-Rod/Linkage Assembly - 4056787050
-Receptacle - WRDK6034 (mounting screws included)
-Ground Lug - 4025101652 (3 total required)
-Ground Lug Mounting Screw - 4020513503 (2 total required)


CTA-ID : 2019431
Was this helpful?
What can we do to improve the information ?