Technical FAQs

Ask a Question

To what extent is the surface of a indoor load center enclosure rust proofed?

The enclosure is made of cold rolled steel with electrodeposited paint. It will rust if the paint is scratched or removed and bare steel is exposed.

CTA-ID : 2019425
Was this helpful?
What can we do to improve the information ?