Technical FAQs

Ask a Question

Customer needs lugs for (1) 750 kcmil for P frame Powerpact Breaker, 400 amp and less.

The CYA400P7 and YA400P7 compression lug kits will accept (1) 500 kcmil to 750 kcmil conductor. 75 degree C 750 kcmil copper conductors are rated for 475 A. Per NEC 240-3, this lug kit can be used on Powerpact P frame breakers with an Ir or Long time setting at or below 500 A if the requirements of NEC 240-6(c) are met. If the requirements of NEC 240-6(c) are not met, the sensor rating must not exceed 400A when using this lug kit.
With aluminum conductors, they can be used on a breaker with an ampere rating of 400 A maximum if the requirements of NEC 240-6(c) are met. If the requirements of NEC240-6(c) are NOT met, the maximum sensor rating permitted is 400 A.



CTA-ID : 2019665
Was this helpful?
What can we do to improve the information ?