Technical FAQs

Ask a Question

Does the QMB363T, Series D2 come with mounting hardware?

Issue:
Product Design Features

Product Line:
QMB Branch Safety Switches

Environment:
Mounting hardware

Cause:
Installation

Resolution
The QMB363T Series D2 switch, comes with a rail extension assembly which is required to attach to the interior side rails in order to mount the switch. It does NOT come with a plug-on extension assembly, which is required if this is to be mounted in a Switchboard or 38" wide enclosure (See the Supplemental Digest Pages 13-4 &.13-5 for more information). The Plug on Extension Assembly is catalog number QMB310EX.



CTA-ID : 2019656
Was this helpful?
What can we do to improve the information ?