Technical FAQs

Ask a Question

Is the NQOD door lock cylinder key slot in the horizontal or vertical position when the door is locked?

The key slot will be vertical when locked.


REVISED 7/9/04


CTA-ID : 2019123
Was this helpful?
What can we do to improve the information ?