Technical FAQs

Ask a Question

The H465 has a footnote in the 173 digest stating ``600 vac only``. Can it be used at 240 volts?

Yes but must use 600 vac fuses. The ``600 vac only`` footnote is intended to mean that it should not be used for DC applications.


CTA-ID : 2019120
Was this helpful?
What can we do to improve the information ?