Technical FAQs

Ask a Question

Can we build a two section nonlinear I-Line panel?

Issue:
Can we build a two section  nonlinear I-Line  panel?  

Product Line:
I line panelboard.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The I-Line panel neutrals do not have sufficient capacity for use in nonlinear multi section construction. The panel should be built as two separate non linear panels.


CTA-ID : 2019117
Was this helpful?
What can we do to improve the information ?