Technical FAQs

Ask a Question

What heaters are recommended for a control voltage of 208 or 240 VAC rather than the standard 120 VAC requirement?

If 120 VAC cannot be provided (120VAC promotes long heater life), wire two heaters in series and add a thermostat if this results in too much heat.

CTA-ID : 2019966
Was this helpful?
What can we do to improve the information ?