Technical FAQs

Ask a Question

Is the LA400R circuit breaker enclosure suitable for service entrance?

Issue:
Product Design Features

Product Line:
Circuit Breaker Enclosures

Cause:
Application

Resolution:
Yes, the device is marked as 'Suitable for use as service equipment'. The code would normally require either a service ground or bonded solid neutral to be installed.


CTA-ID : 2019099
Was this helpful?
What can we do to improve the information ?