Technical FAQs

Ask a Question

Can an 800A P frame circuit breaker be installed in an existing or current HCW vertical mount main breaker interior?

The P frame circuit breaker cannot be installed in either an existing or current HCW vertical mount main breaker interior for a couple of reasons. The deadfront is not designed to support the use of a P frame circuit breaker. There is also no labeling to support its use.


CTA-ID : 2019951
Was this helpful?
What can we do to improve the information ?