Technical FAQs

Ask a Question

Can a control transformer be installed into an 8536SAG enclosure?

Issue:     
Control power transformer field addition 

Product Line: 
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Adding a control power transformer to size 00 NEMA 1 enclosed starter


Resolution:
No the Nema 1 slip on enclosures do no provide enough room for the transformer and fusing. The enclosure for use with a control transformer is a 9991SCG1

This is also true for the 8502 and 8536 type S size 0, and 1 devices. 

 
Was this helpful?
What can we do to improve the information ?