Technical FAQs

Ask a Question

What is the ambient temperature rating of an 8910DPA contactor?

The temperature rating is 0 to 65 C or 149 F.



CTA-ID : 2020350
Was this helpful?
What can we do to improve the information ?