Technical FAQs

Ask a Question

Will the new Micrologic Por H trip unit protect against the loss of one phase?

The P or H trip unit will not detect the loss of one phase. You would need an external relay for phase loss protection.
It will protect against undervoltage if the threshhold is set no lower than 80%.


CTA-ID : 2019356
Was this helpful?
What can we do to improve the information ?