Technical FAQs

Ask a Question

What is the neutral rating on a piece of busway CP506G10?

The neutral bars are 100% rated, or 600A on that busway.


CTA-ID : 2019353
Was this helpful?
What can we do to improve the information ?