Technical FAQs

Ask a Question

What is the required bus-mounting torque for an MAF circuit breaker?

The bus mounting torque for the MAF MHF MAP and MHP is 225 - 250 lb.-in. or 25.4 - 28.3 N.m


CTA-ID : 2020333
Was this helpful?
What can we do to improve the information ?