Technical FAQs

Ask a Question

Q1370 Circuit Breaker Replacement

Issue:
What is the replacement for a Q1370 circuit breaker in the obsolete NQO panelboard?

Product Line:
Obsolete NQO panelboards that were sold and supported in the USA.

Environment:
Replacement/maintenance.

Cause:
Is there  a replacement for the Q1370 circuit breaker in the obsolete NQO panelboards?

Resolution:
Replace with a QO370 in an NQO panelboard.  A QO370 can be installed in an NQO panelboard with an SK5669 mounting assembly.


CTA-ID : 2019876
Was this helpful?
What can we do to improve the information ?