Technical FAQs

Ask a Question

What is the maximum branch breaker applicable to the branch section of a RC816D200CH meter main?

A 100 ampere maximum Homeline branch circuit breaker may be installed in the lowest position in the branch panel. All other positions are limited to 70 ampere maximum.


CTA-ID : 2019593
Was this helpful?
What can we do to improve the information ?