Technical FAQs

Ask a Question

What size wire would the H225N series E1 neutral assembly handle?

The neutral assembly H600SN is used in the H225N. The H600SN wire range is (4) 750 kcmil maximum copper or aluminum. & 1 300 kcmil maximum aluminum or copper.

CTA-ID : 2019343
Was this helpful?
What can we do to improve the information ?