Technical FAQs

Ask a Question

What is the standard ambient operating temperature range for the XY2CE... and XY2CH... cable pull switch?

It is -13 Degree F (-25 Degree C) to 158 Degree F (70 Degree C).


CTA-ID : 2019308
Was this helpful?
What can we do to improve the information ?