Technical FAQs

Ask a Question

What is 2510FW8?

This is a special which is similar to the 2510FW2 but supplied with FR type enclosure with gasketed cover and a 0 ring on the shaft,. NEMA 4 rated device with glyptal applied to the internal operator.


CTA-ID : 2020320
Was this helpful?
What can we do to improve the information ?