Technical FAQs

Ask a Question

What is the minimum operating temperature for the Phaseo ABL Power Supplies?

These can be operated between 32 to 140 degrees F (0 - +60 degrees C) derating 122 degrees F (50*C)


CTA-ID : 2020303
Was this helpful?
What can we do to improve the information ?