Technical FAQs

Ask a Question

What components were included with a GS504NI? What replaces it?

Selection, Product Features

Product Line:
Medical Panels

NFPA99, NEC517.160

For a complete installation, all required components must be included or accounted for in the design.

NOTE:  GS504NI is obsolete and replaced by SGPMG4NN0.  Both obsolete and current device fit a 4 gang box.  The GS504NI included a 4 gang stainless steel trim with 4 ground receptacles. It did not include the back box which was provided by the installer.

CTA-ID : 2020298
Was this helpful?
What can we do to improve the information ?