Technical FAQs

Ask a Question

Powerpact Q frame circuit breakers have hold and trip values. Is this adjustable?

No. It is a fixed setting. It will always hold below the hold value. May or may not trip between the hold and trip value. Will always trip above the trip value.


CTA-ID : 2019873
Was this helpful?
What can we do to improve the information ?