Technical FAQs

Ask a Question

What is the ampere rating of the SS4BLC bus link kit for use in a Class 2730 CTC assembly?

One SS4BLC bus link kit is rated 600A maximum. If the ampere rating of the CTC assembly is over 600A, two bus link kits would be required.

CTA-ID : 2019856
Was this helpful?
What can we do to improve the information ?