Technical FAQs

Ask a Question

What is the length of the shaft on a XB5 reset mechanism ?

The actuation distance is between 17 & 120mm or 120 & 257mm The length of the shaft can be adjusted by cutting. The travel distance is 10mm.

CTA-ID : 2019564
Was this helpful?
What can we do to improve the information ?