Technical FAQs

Ask a Question

What is used to fasten two straight lengths of trench duct together?

A coupler consists of two 45206-176-50, one of which is required on each side rail of the trench duct. Couplers are furnished on one end of each straight section and fitting.

CTA-ID : 2019305
Was this helpful?
What can we do to improve the information ?